unl_cpu
iunl_cpu
ER unl_cpu (void);ER iunl_cpu (void);Note 1 These service calls do not perform queuing of cancellation requests. If the system is in the CPU unlocked state, therefore, no processing is performed but it is not handled as an error.
Note 2 These service calls do not cancel the dispatching disabled state that was set by issuing dis_dsp.