vrst_mbf
ER vrst_mbf (ID mbfid);The messages having been accumulated by the message buffer area are annulled. The tasks to wait to send message to the target message buffer are released from the WAITING state, and EV_RST is returned as a return value for the tasks.
Note 1 In this service call, the tasks to wait to receive message do not released from the WAITING state.