wai_flg

Outline

Wait for eventflag (waiting forever).

C format

 ER      wai_flg (ID flgid, FLGPTN waiptn, MODE wfmode, FLGPTN *p_flgptn);
Parameter(s)

I/O

Parameter

Description

I

 ID      flgid;
ID number of the eventflag.

I

 FLGPTN  waiptn;
Wait bit pattern.

I

 MODE    wfmode;
Wait mode.

TWF_ANDW: AND waiting condition.

TWF_ORW: OR waiting condition.

O

 FLGPTN  *p_flgptn;
Bit pattern causing a task to be released from waiting.



Explanation

This service call checks whether the bit pattern specified by parameter waiptn and the bit pattern that satisfies the required condition specified by parameter wfmode are set to the eventflag specified by parameter flgid.

If a bit pattern that satisfies the required condition has been set for the target eventflag, the bit pattern of the target eventflag is stored in the area specified by parameter p_flgptn.

If the bit pattern of the target eventflag does not satisfy the required condition when this service call is issued, the invoking task is queued to the target eventflag wait queue.

As a result, the invoking task is unlinked from the ready queue and is moved from the RUNNING state to the WAITING state (WAITING state for an eventflag).

The WAITING state for an eventflag is cancelled in the following cases.

WAITING State for an Eventflag Cancel Operation

Return Value

A bit pattern that satisfies the required condition was set to the target eventflag as a result of issuing set_flg.

E_OK

A bit pattern that satisfies the required condition was set to the target eventflag as a result of issuing iset_flg.

E_OK

Forced release from waiting (accept rel_wai while waiting).

E_RLWAI

Forced release from waiting (accept irel_wai while waiting).

E_RLWAI



The following shows the specification format of required condition wfmode.

- wfmode == TWF_ANDW
Checks whether all of the bits to which 1 is set by parameter waiptn are set as the target eventflag.

- wfmode == TWF_ORW
Checks which bit, among bits to which 1 is set by parameter waiptn, is set as the target eventflag.

Note 1 With the RI600V4, whether to enable queuing of multiple tasks to the event flag wait queue is defined during configuration. If this service call is issued for the event flag (TA_WSGL attribute) to which a wait task is queued, therefore, "E_ILUSE" is returned regardless of whether the required condition is immediately satisfied.

TA_WSGL: Only one task is allowed to be in the WAITING state for the eventflag.

TA_WMUL: Multiple tasks are allowed to be in the WAITING state for the eventflag.

Note 2 Invoking tasks are queued to the target event flag (TA_WMUL attribute) wait queue in the order defined during configuration (FIFO order or current priority order).
However, when the TA_CLR attribute is not specified, the wait queue is managed in the FIFO order even if the priority order is specified. This behavior falls outside mITRON4.0 specification.


Note 3 The RI600V4 performs bit pattern clear processing (0 setting) when the required condition of the target eventflag (TA_CLR attribute) is satisfied.

Return value

Macro

Value

Description

E_OK

0

Normal completion.

E_PAR

-17

Parameter error.

- waiptn == 0

- wfmode is invalid.

E_ID

-18

Invalid ID number.

- flgid < 0

- flgid > VTMAX_FLG

E_CTX

-25

Context error.

- This service call was issued from a non-task.

- This service call was issued in the CPU locked state.

- This service call was issued in the dispatching disabled state.

- This service call was issued in the status "PSW.IPL > kernel interrupt mask level".

E_ILUSE

-28

Illegal use of service call.

- There is already a task waiting for an eventflag with the TA_WSGL attribute.

E_RLWAI

-49

Forced release from the WAITING state.

- Accept rel_wai/irel_wai while waiting.