These service calls change the priority of the task specified by parameter 
tskid (current priority) to a value specified by parameter 
tskpri.
 
 Note If the target task is in the RUNNING or READY state after this service call is issued, this service call re-queues the task at the end of the ready queue corresponding to the priority specified by parameter 
tskpri, following priority change processing.