1.7 Free Evaluation Editions

The free evaluation editions have a trial period of 60 days from the day of the first building by the compiler over which you can use features equivalent to those of the Professional editions.

After that period, the additional features of the Professional editions are no longer available, and a restriction becomes applicable to the sizes produced by linkage.

-

The restriction on the section sizes which can be allocated to the ROM area is up to 256 Kbytes in total. A linker error occurs when the size exceeds 256 Kbytes.

 

The version number of the optimizing linkage editor is prefixed by W while a compiler is operating as an evaluation edition and by V when it is operating as a commercial edition.

Examples are given below.

-

Version of a free evaluation edition:

Renesas Optimizing Linker W1.01.01 [25 Apr 2014]

-

Version of a commercial edition:

Renesas Optimizing Linker V1.01.01 [25 Apr 2014]

 

We do not supply the following services for the evaluation editions.Consider purchasing a commercial edition if you require them.

-

Technical support

-

E-mail delivery of items such as information on revisions