This option changes an external symbol name or a section name.
-REName={[file](name1=name2[,name1=name2]...)|[module](name1=name2[,name1=name2]...)}[[,{[file](name1=name2[,name1=name2]...)|[module](name1=name2[,name1=name2]...)}]...] |
Specify the symbol name or section name to be changed as name1. Specify the symbol name or section name after changing as name2. |
Symbol names or section names in specific file file or a module in specific library module can be changed. |
If there are two or more files or modules with the same name, the priority depends on the input order. |
If this option is specified together with the -extract option or -strip option, this option will be invalid. |
When the -form=absolute option is specified, the section name of the input library cannot be changed. |
Operation is not guaranteed if this option is used in combination with compile option -Xmerge_files. |