4.1.5
Option to process in strict accordance with ANSI standard
If the -Xansi option is specified to CC-RH, it will perform processing in strict accordance with the ANSI standard. The differences between when the -Xansi option is specified and when not specified are as follows.
Table 4.8 | Processing When -Xansi Option Strictly Conforming to Language Specifications is Specified |
|
|
|
|
|
Bit field
|
An errorNote 1 occurs if type other than int is specified for bit field.
|
Specification of types other than int is allowed.
|
|
# line number
|
An error occurs.
|
Treated in same manner as "#line line number".Note 2
|
|
Parameters of functions declared with #pragma inline
|
If the type of a return value or parameter is different but type conversion is possible between the specified function call and definition, then an error will occur.
|
The type of the return value is converted to the type at the call site, the parameters are converted to the type of the function definition, and inline expansion is performed.
|
|
__STDC__
|
Defines value as macro with value 1.
|
Does not define.
|
|
_Bool type
long long type
|
An error occurs.
|
Specification is allowed.
|
|
Structure and union specifiers
|
If the member declaration list does not include named members, then an error message will be output indicating that the list has no effect.
|
If the member declaration list does not include named members, then an warning message will be output indicating that the list has no effect.
|
Note 1. | Normal error beginning with "E". The same applies hereafter. |
Note 2. | See the ANSI standards. |