.line


Line-number information from the C source program.

[Syntax]

Symbol field
Mnemonic field
Operand field
Comment field
 
.line 
["file-name",] line-number
[; comment]

[Function]

-

The .func directive is compiler debugging information.

[Description]

-

Modifies the line numbers and filenames referenced during debugging.

-

The line numbers and filenames in the source program are not updated between the first .line directive and the next one.

-

If the filename is omitted, then only the line number is changed.

-

This is the line-number information of the C source program that the compiler outputs. A change made in the assembly source file is invalid.