Renesas Electronics
top
Compiler
COMMAND REFERENCE
Option
Assemble options
Optimization
Optimization
The optimization option is as follows.
-
-goptimize
Previous Topic
-mirror_region
Next Topic
-goptimize
Table of Contents
Version/help display specification
Output file specification
Source debugging control
Device specification control
Optimization
-goptimize
Symbol definition specification
Include file reading path specification
Input file control
Assembler transition support
Error message file output specification
Warning message output control
Subcommand file specification