This option outputs the variable/function information file.
[Specification format]
- | Interpretation when omitted |
The variable/function information file is not output.
[Detailed description]
- | Specify the variable/function information file as file. |
- | If the file name is omitted, vfinfo.h is output as the variable/function information file. |
- | When the file name has no extension, ".h" is assumed as the extension. |
[Example of use]
- | To output the variable/function information file to file.h, describe as: |
>rlink a.obj b.obj -vfinfo=file.h
|
[Remark]
- | If the -form={object|relocate|library} option, -strip option, or -extract option is specified, this option will be invalid. |
- | If the -device option is not specified, this option will be invalid. |
- | When the section allocation address exceeds the allowable address range, information regarding only the symbols and sections allocated within the allowable areas are output to the variable/function information file. [V1.04 or later] |