-Absolute_forbid


This option disables optimization regarding address + size specification.

[Specification format]

-Absolute_forbid=address[+size][,address[+size]]...

 

-

Interpretation when omitted

Optimization regarding address + size specification is not disabled.

[Detailed description]

-

This option disables optimization regarding address + size specification.

-

Specify the hexadecimal address and size for address and size.

[Example of use]

-

To disable optimization for addresses 0x1000 to 0x11ff, describe as:

>rlink a.obj b.obj -optimize -absolute_forbid=1000+200

[Remark]

-

This option is ignored if optimization is not applied at linkage.