Conversion of character string to flonptrating-point number (double type) and storing pointer in last character string
double __far strtod(const char __near *nptr, char __near * __near *endptr);
double __far _COM_strtod_ff(const char __far *nptr, char __far * __far *endptr);
If the partial character string has been converted, the resultant value is returned. If the character string could not be converted, 0 is returned.
If an overflow occurs , strtod returns ±∞ and sets macro ERANGE to global variable errno.
If an underflow occurs, strtod returns 0 and sets macro ERANGE to global variable errno.
This function skips 0 or more columns of white-space characters (character which makes the isspace function true) from the start of the string indicated by nptr, and converts the string from the next character into a double-type representation. When endptr is not the null pointer, the pointer to the remaining strings that were not converted is set to endptr.