< Compile Options / Optimize Options >
When the speed option is specified, optimization will be performed with emphasis on execution performance. |
When the speed option is specified, the following options are automatically specified based on the optimize option specification. |
The processing for optimization in response to the optimization level selected for the optimize option includes the fine adjustment of many items other than those that can be specified through compiler options. Code produced with different levels of optimization will differ in the ways set by the compiler options listed in the tables below, but will also not match in other ways. |
<When optimize=max is specified>
The default is map when a C/C++ source program has been specified for input and output=abs or output=mot has been specified for output. For any other case, the default is nomap. |
<When optimize=2 is specified>
<When optimize=0 or optimize=1 is specified>