1.2 Features

Below are the features of the resource information tool.



- Confirm RI600V4 resource information

When the program running in the debugging tool is stopped at an arbitrary location, the current status of the RI600V4 resource information appears in the Realtime OS Resource Information panel.