[Data Queue] tab

This tab displays the data queue information (e.g. Data Queue Name and ID) of the RI600V4.

Figure A-10. [Data Queue] Tab



The following items are explained here.

- [How to open]

- [Description of each area]

- [Context menu]

[How to open]

- From the [Debug] menu, select [Download].

- From the [View] menu, select [Realtime OS] >> [Resource Information].

[Description of each area]

(1) Information display area

(a) First layer

This layer displays the data queue information (e.g. Data Queue Name and ID) of the RI600V4.

This layer consists of the following items.

Data Queue Name

An icon indicating the current status of the data queue and the name of the data queue are shown in the following format.

Icon Name

There are queued tasks (sending waiting tasks).

There are queued tasks (receiving waiting tasks).

There are queud data (receiving waiting data).

There are no queued tasks/data (waiting tasks/receiving waiting data).

ID

The ID of the data queue is shown.

Queue Status

The current status of the data queue is shown.

Waiting Tasks (Send)

There are queued tasks (sending waiting tasks).

Waiting Tasks (Receive)

There are queued tasks (receiving waiting tasks).

Waiting Data

There are queud data (receiving waiting data).

Empty

There are no queued tasks/data (waiting tasks/receiving waiting data).

Total Buffers

Displays the maximum number of data buffers that can be queued.

Free Buffers

Displays the number of free buffers in the data queue.

The number of free buffers is the total number of buffers minus the number of buffers receiving waiting data.

Number of Data

The number of data stored in the data queue.

Attribute

Displays the queuing method of the sending waiting tasks.

If the queuing method if the receiving waiting tasks is "data reception request order", then the queuing method of the receiving waiting data will be "data send request order".

TA_TFIFO

FIFO order

TA_TPRI

Task priority order



(b) Second layer

<1> Sending waiting task/receive waiting task information

The sending/receiving waiting task information (e.g. Task Name and ID) only appears if there are tasks queued in the data queue's wait queue.

See the [Task] tab for details about sending/receiving waiting task information.

Figure A-11. [Data Queue] Tab (Sending Waiting Task Information)



Figure A-12. [Data Queue] Tab (Receiving Waiting Task Information)



<2> Receiving waiting data information

The receiving waiting data information (e.g. Data) only appears if there are data queued in the data queue.

Figure A-13. [Data Queue] Tab (Receiving Waiting Data Information)



This area consists of the following items.

Data

the contents of the data is shown.



[Context menu]

The context menu displayed in response to a right mouse click differs as follows depending on the area clicked.

(1) Header row

Display

Displays cascade menus for selecting the header items to display.

Selected item name

The following items are displayed for selection.

Data Queue Name, ID, Queue Status, Total Buffers, Free Buffers, Number of Data, Attribute

Checked

The item in question will be displayed.

Not checked

The item in question will not be displayed.

Notation

Displays cascade menus for selecting the display notation.

Selected item name

The following items are displayed for selection.

ID, Total Buffers, Free Buffers, Number of Data

DEC

Displays value in signed decimal number.

HEX

Displays value in hexadecimal number.



(2) Footer row

Reset Display Item

Resets the item displayed to initial state.