[Memory Area] tab

This tab displays the memory area information (e.g. Area Name and Top Address) of the RI78V4.

Figure A-3. [Memory Area] Tab



The following items are explained here.

- [How to open]

- [Description of each area]

- [Context menu]

[How to open]

- From the [Debug] menu, select [Download].

- From the [View] menu, select [Realtime OS] >> [Resource Information].

[Description of each area]

(1) Information display area

This area displays the memory area information (e.g. Area Name and Top Address) of the RI78V4.

This area consists of the following items.

Area Name

An icon and the name of the managed memory area are shown in the following format.

Icon Name

kernel_system

Area where kernel codes are to be allocated.

kernel_system_timer_n

Area where the system timer code and the infomation of far branch code for interrupt handler are to be allocated.

kernel_info

Area where information items such as the RI78V4 version are to be allocated.

kernel_const

kernel_const_f

Area where initial information items related to OS resources that do not change dynamically are allocated as system information tables.

kernel_stack

Area where the system stack and the task stack are to be allocated.

kernel_data

Area where managed objects for RI78V4 are to be allocated.

kernel_data_init

Area where information itemes related to RI78V4 initialization.

kernel_workn

Area where fixed-sized memory pools are to be allocated.

kernel_data_trace_n

kenrel_const_trace_f

Area where the trace data and information necessary to get the trace data are to be allocated.

kernel_system_trace_f

Area where the codes for getting the trace data are to be allocated.

kernel_sbss

Area of SADDR for RI78V4

Top Address

The start address of the managed memory area is shown.

Size

The size of the managed memory area (in bytes) is shown.



Remark If the memory area information (e.g. Area Name and Top Address) in each cell is double clicked, then Memory panel displays the contents of the managed memory area, and the caret moves to the corresponding location.

[Context menu]

The context menu displayed in response to a right mouse click differs as follows depending on the area clicked.

(1) Header row

Display

Displays cascade menus for selecting the header items to display.

Selected item name

The following items are displayed for selection.

Area Name, Top Address, Size

Checked

The item in question will be displayed.

Not checked

The item in question will not be displayed.

Notation

Displays cascade menus for selecting the display notation.

Selected item name

The following items are displayed for selection.

Top Address, Size

DEC

Displays value in signed decimal number.

HEX

Displays value in hexadecimal number.



(2) Footer row

Jump to Memory (Top Address)

Opens the Memory panel, and displays the contents of the managed memory area.

Reset Display Item

Resets the display item (e.g. whether or not to display header items, display notation, display order and display width).