ServiceCall dialog box

Execute a service call process.

Figure A-32. ServiceCall Dialog Box



The following items are explained here.

- [How to open]

- [Description of each area]

[How to open]

- From the Realtime OS Resource Information panel context menu, select [Service Call] >> [Service Call Name].

[Description of each area]

(1) Service call display area

This area displays the service call selected in the context menu, in C format.

Remark If the service call requires a value to be input, a text box will appear in this area. Enter the value in question, then click [OK] to run the service call process.

(2) Function button

Button

Function

OK

Execute a service call process.

Cancel

Ignore the setting and closes this dialog box.

The function of this item is same as that of the button.