The following are the features of the debugger provided by CS+.
Synchronous execution and synchronous break in a microcontroller that supports multi-core |
A pleasant debugging environment for target systems is provided by connecting to the full-spec emulator (Full-spec emulator), the on-chip debugging emulator (E1/E20) and Simulator.
The C source text and the disassembled text are shown mixed on the same panel.
The source level debugging and the instruction level debugging for a C source program can be done.
The code flash can be rewrote by using the flash self library of the flash self programming function.
The contents of memory, registers and variables are automatically updated not only when the program execution is stopped, but also in execution.
The debugging environment such as breakpoints, event configuration information, file download information, display condition/position of the panel, etc. can be saved.