2.3.5.4 [Flash Options Settings] tab

You can configure options for the flash memory incorporated in the microcontroller.

Note that this tab appears only when the selected microcontroller supports the flash options.

To configure options, specify the corresponding items via the Flash Options Setting dialog box, that is opened by clicking the [...] button appears at the right of the field by selecting the [Flash options] property in the [Flash Options] category on this tab (the [...] button appears only while connected to the debug tool).

See the Flash Options Setting dialog box for details on the configuration.

Figure 2.61

Opening Flash Options Setting Dialog Box

Figure 2.62

Flash Options Settings (Flash Options Setting Dialog Box)