2.4.2  
Disconnect from the debug tool 
 
By clicking the  button on the Debug toolbar, CS+ cuts off the communication with the connected debug tool.
 button on the Debug toolbar, CS+ cuts off the communication with the connected debug tool. 
After disconnecting from the debug tool, the Statusbar of the Main window changes as follows:
| 
Figure 2.64 | Statusbar Indicating Disconnection from Debug Tool | 
| 
Caution | The debug tool cannot be disconnected from CS+ while the program is running. | 
| 
Remark | Disconnecting the debug tool will close all the panels and dialog boxes that can be displayed only during the connection. |