2.4.2
Disconnect from the debug tool
By clicking the
button on the Debug toolbar, CS+ cuts off the communication with the connected debug tool.
After disconnecting from the debug tool, the Statusbar of the Main window changes as follows:
Figure 2.64 | Statusbar Indicating Disconnection from Debug Tool |
Caution | The debug tool cannot be disconnected from CS+ while the program is running. |
Remark | Disconnecting the debug tool will close all the panels and dialog boxes that can be displayed only during the connection. |