Execute the program (see "2.8 Execute Programs").
When an instruction for which a timer start event or a timer end event has been set is executed, a timer measurement is started or finished.
After the program is stopped, the result of the measurement is displayed in the Events panel opened by selecting the [View] menu >> [Event], in event type as "Timer Result".
This Timer Result is a particular type of event that is displayed on only the Events panel when either a timer start event or a timer end event has been set.
Example of Result of Timer Result Event (Timer Start Event/Timer End Event) [Full-spec emulator][E1][E20] |