The execution history is collected as trace data only for a section while the program is in execution by setting a Trace event.
This Trace event consists of a trace start event and a trace end event.
To use this function, follow the procedure described below.
Also see "2.17.6 Notes for setting events" for details on Trace events (e.g. limits on the number of enabled events). |