The core (PE) to be debugged can be selected in either of the following two ways.
Select a desired PE from the drop-down list (shown below) on the statusbar in the Main window.
Select a desired PE on the Debug Manager panel that are opened by selecting [Debug Manager] from the [View] menu.