2.8.1 Reset microcontroller (CPU)

To reset CPU, click the button on the debug toolbar.

When CPU is reset, the current PC value is set to the reset address.

Remark 1.

You can automatically overwrite the value of I/O register/CPU register with the specified values after CPU reset under breaking (see "2.18 Use Hook Function" for details).

Remark 2.

In cases of failure to reset, the following setting may be required to enable resetting.

-

The [Reset While Running] category on the [Debug Tool Settings] tab of the Property panel

[Use the force reset] property

[Yes]