2.2.1.2 [E1]

Connect a host machine and E1. If required, connect a target board, too.

See E1 User's Manual for details on the connection method.

Figure 2.2

Connection Example [E1]

Caution

Only serial communications are supported as the communication method with the target board (JTAG communications is not available).