To search the collected trace data, click the 
 button to open the Trace Search dialog box (note that the search is disabled during execution of a program). 
In this dialog box, follow the steps below.
When the tab on the tab selection area is selected, the trace data can be searched in instruction level/source level.
Note however, that if you search the trace data at the instruction level, the display mode must be set in the Trace panel to the Mixed display mode or Disassemble display mode.
When searching at the source level, the mode must be set to the Mixed display mode or Source display mode.
This section describes the following.