2.15.7.2
Event types that can be set and deleted during execution
Types of events that can be set or removed during execution of the program or during execution of the tracer/timer are described below.
The meaning of each mark in the table below is as follows:
|
|
Possible
|
|
|
Possible, if the program execution is allowed to pause for events
(Property panel >> [Debug Tool Settings] tab >> [Set Event While Running] category >> [Set event by stopping execution momentarily] property >> [Yes])
|
|
|
Impossible while tracer or timer is executing
|
|
|
Impossible, or not supported
|
Table 2.21 | Event Types That Can be Set and Deleted during Execution |
|
|
|
|
|
|
|
|
|
|
|
|
|
|
Hardware Break
(before execution)
|
|
|
|
|
|
|
Hardware Break
(after execution)
|
|
|
|
|
|
|
Hardware Break
(access)
|
|
|
|
|
|
|
Software Break
|
|
|
|
|
|
|
Trace
(trace start/trace end)
|
|
|
|
|
|
|
Point Trace
|
|
|
|
|
|
|
Timer Result
(timer start/timer end)
|
|
|
|
|
|
|
Action (Printf)
|
|
|
|
|
|