2.6.2.1 Change display mode

You can change the display mode of the Disassemble panel by clicking the button (toggle) on the toolbar.

(1)

Mixed display mode

In this display mode (default), the disassembled text is displayed combined with the source text.

Figure 2.64

Mixed Display Mode (Disassemble Panel)

(2)

Disassemble display mode

In this display mode, the source text is hidden and only the disassembled text is displayed.

Figure 2.65

Disassemble Display Mode (Disassemble Panel)