2.8.1.1 [IECUBE]

Figure 2.71

[Break] Category [IECUBE]

(1)

[First using type of breakpoint]

Specify the type of preferential breakpoint with a single click of the mouse in the Editor panel/Disassemble panel.

Select from the drop-down list below for each use of the breakpoint.

Hardware break

Sets hardware breakpoint with priority, by using the Hardware break function.

Once set, it is treated as a Hardware Break event (execution system).

Software break

Sets software breakpoint with priority, by using the Software break function (except for [Simulator]) (default).

Once set, it is treated as a Software Break event.

Caution

If the number of the set breakpoints of the specified type exceeds the limit settable (see "2.15.7.1 Maximum number of enabled events"), a breakpoint of another type will be used.

(2)

[Stop emulation of timer group when stopping]

Select whether to terminate the peripheral emulation of timers while stopping the program execution (Peripheral Break).

Select [Yes] to terminate (default: [No]).

(3)

[Stop emulation of serial group when stopping]

This property appears only when the selected microcontroller supports the function that terminates the peripheral emulation of serials (Peripheral Break).

Select whether to terminate the peripheral emulation of serials while stopping the program execution.

Select [Yes] to terminate (default: [No]).

(4)

[Use open break function]

This property appears only when the selected microcontroller supports the open break function.

Select from the following drop-down list whether to use the open break function.

The default value depends on the type of the selected microcontroller.

Yes(Hi-Z)

The open break target pin becomes the Hi-Z state after the CPU is stopped.

No(Output signal)

The open break target pin outputs the signal even after the CPU is stopped.