The cause of the break other than the described above is as follows:
You can confirm the break cause with the Status message on the statusbar in the Main window.
Table 2.6 | Other Break Causes |
|
|
|
|
|
|
|
|
Full of the trace memoryNote 1
|
|
|
|
|
An occurrence of Trace Delay Break
|
|
|
|
|
Execution time-over detected
|
|
|
|
|
An access to non-mapped area
|
|
|
|
|
A writing to write-protected area
|
|
|
|
|
An access to the odd number address by the word width
|
|
|
|
|
An occurrence of Temporary BreakNote 2
|
|
|
|
|
An occurrence of Flash Illegal Break
|
|
|
|
|
Illegal action of program related to the peripheral chip functionNote 3
|
|
|
|
|
Failure to execute/uncertain cause
|
|
|
|
|
Full of the current consumption bufferNote 4
|
|
|
|
Note 2. | A break that is internally used by CS+. (Users cannot use it.) |
Note 3. | See the documentation on peripheral emulation board to use. |
Note 4. | The operation is supported only by the simulator that supports the current consumption measurement. |