2.17.7.2 Types of events that can be set or removed during execution

Types of events that can be set or removed during execution of the program or during execution of the tracer/timer are as follows:

Table 2.24

Types of Events that Can Be Set or Removed during Execution

Type of event

Debug tool

E1(Serial)/E1(JTAG)
E20(Serial)/E20(JTAG)
EZ Emulator

Simulator

Software break

Note1 Note2

 

Hardware break (execution-related: before execution)

Note2

 

Break event (execution-related: after execution)

Note2

 

Break event (access-related: Read, Write, Read/Write)

Note2

 

Trace (trace start, trace end)

 

 

Point trace

 

 

Timer result (timer start, timer end)

 

 

Action (Printf event)

Note1 Note2

 

Action (Interrupt event)

 

 

: Possible

: Possible if program execution is momentarily halted

: Impossible during tracer execution

: Not supported

: Impossible

Note 1.

Internal RAM area only

Note 2.

Events cannot be set while the microcontroller is in a power-down mode.