2.17.3 Jump to an event address

By clicking one of the following buttons, it is possible to jump to the relevant panel corresponding to the address of a currently selected event.

However, these buttons are disabled when a trace event, timer measurement event, or a built-in event (unconditional trace event or Run-Break timer event) is selected.

 

 

The Editor panel opens, with the caret on it moved to the source line corresponding to the address at which a selected event is set.

 

The Disassemble panel opens, with the caret on it moved to the disassembled result corresponding to the address at which a selected event is set.

 

The Memory panel opens, with the caret on it moved to the memory value corresponding to the address at which a selected event is set.