2.14.2.2 Checking the Events panel for confirmation

When a program has stopped running, the measurement result is displayed as a Run-Break timer event on the Events panel that is opened by selecting [Event] from the [View] menu.

Figure 2.153

Example of a Run-Break Timer Event Measurement Result (Events Panel) [E1] [E20]

Figure 2.154

Example of a Run-Break Timer Event Measurement Result (Events Panel) [Simulator]