2.13.6.1 Changing the display mode

By clicking one of the toolbar buttons shown below, it is possible to change the display mode as suitable for the purpose of use.

However, these buttons are disabled while the trace function is in operation.

Table 2.14

Trace Panel Display Modes

Button

Display Mode

Display Contents

 

Mixed display mode

Instructions (disassemble), label names, source text (corresponding source lines), and point trace results are displayed (default).

 

Disassemble display mode

Instructions (disassemble), label names, and point trace results are displayed.

 

Source display mode

Source text (corresponding source lines) are displayed.

However, if any place that has no debug information is executed, a notice "<No Debug Information>" is displayed.

Figure 2.144

Example of Source Display Mode (Trace Panel)