2.6.2.2 Changing the display form

The form in which disassembled results are displayed can be changed freely by using the toolbar buttons shown below.

View

Shows the following buttons that change the display form.

 

 

Displays the offset values of labels. If the address has no labels defined, an offset value from the closest label is displayed.

 

Displays address values in the form "symbol + offset value" (default).

However, if the address value has a symbol defined, only the symbol is displayed.