2.6.4 Performing line assembly

The instructions and instruction codes displayed on the Disassemble panel can be edited (line-assembled).

Following methods of operation are described here.

 

2.6.4.1 Editing instructions

2.6.4.2 Editing instruction code