2.11.6.8 Exporting/importing watch-expressions

This feature allows you to export currently registered watch-expressions to a file and import it so that the watch-expressions can be re-registered.

To do this, follow the procedure described below.

(1)

Export watch-expressions

Save watch-expressions currently being registered (including categories) in a file format that is possible to import.

While the focus is in the Watch panel, select [Save Watch Data As...] from the [File] menu.

On the Save As dialog box that is automatically opened, specify the following items, and then click the [Save] button.

-

[File name]: Specify the name of a file to be saved (the file extension must be "csv").

-

[Save as type]: Select "Importable CSV (Comma-Separated Variables)(*.csv)".

Caution

Neither values nor the type information of watch-expressions can be saved.
Items that are expanded after analyzing watch-expressions (i.e. an array, structure, and so on) cannot be saved.

Figure 2.133

Export of Watch-Expressions

(2)

Import watch-expressions

Import the file that was exported in (1) to the Watch panel.

On the Watch panel to which you want to import watch-expressions, select [Import Watch Expression...] from the context menu.

On the Open Watch Expression Data File dialog box that is automatically opened, specify the exported file, and then click the [Open] button.

Remark

If watch-expressions have been already registered, then imported watch-expressions will be registered at the bottom of them.

Figure 2.134

Import of Watch-Expressions