This dialog box is used to select a file-encoding.
Figure A.6  | Encoding Dialog Box  | 
 
 
This section describes the following.  
[How to open]
-  | From the [File] menu, open the Open File dialog box by selecting [Open with Encoding...], and then click the [Open] button in the dialog box.  | 
 
[Description of each area]
Select the encoding to be set.
The encoding of the selected file is selected by default.
[Function buttons]
| 
 | 
 | 
| 
 
OK 
 | 
 
Opens the selected file in the Open File dialog box using a selected file encoding. 
 | 
| 
 
Cancel 
 | 
 
Not open the selected file in the Open File dialog box and closes this dialog box. 
 | 
| 
 
Help 
 | 
 
Displays the help for this dialog box.  
 |