The columns or marks displayed on the Editor panel can be set by selecting the toolbar items shown below.
Note that this setting applies to all of the Editor panels.
| 
 The following items are displayed to show or hide the columns or marks on the Editor panels. Remove the check to hide the items (all the items are checked by default).  | 
||
| 
 Shows the mark that indicates the line modification status, in the line number area.  | 
||
| 
 Shows the mark that indicates the update status of the downloaded load module file, in the line number area. Note that this item is enabled only when connected to the debug tool.  | 
||
| 
 Note that this item is enabled only when connected to the debug tool.  | 
||
| 
 Note that this item is enabled only when connected to the debug tool.  | 
||
| 
 Note that this item is enabled only when connected to the debug tool and the Mixed display mode is selected.  | 
||
| 
 Note that this item is enabled only when connected to the debug tool and the Mixed display mode is selected.  | 
||
| 
 Note that this item is enabled only when connected to the debug tool.  | 
||