>>>info = debugger.Map.Information() ...Execute Map.Information function
1: 0x00000000 0x0003FFFF 32 (Internal ROM area)
2: 0x00040000 0x00048FFF 8 (Non map area)
3: 0x00049000 0x001003FF 8 (Emulation ROM area)
4: 0x00100400 0x03FF8FFF 8 (Non map area)
5: 0x03FF9000 0x03FFEFFF 32 (Internal RAM area)
6: 0x03FFF000 0x03FFFFFF 8 (I/O register area)
>>>print info[0].StartAddress
0
>>>print info[0].EndAddress
262143
>>>print info[0].AccessSize
32
>>>print info[0].MapTypeName
Internal ROM area
>>>print info[5].StartAddress
67104768
>>>print info[5].EndAddress
67108863
>>>print info[5].AccessSize
8
>>>print info[5].MapTypeName
I/O register area
>>>
|