VariableInfo


This class holds variable information (return value of the project.GetVariableList function).

[Type]

class VariableInfo:
        VariableName = None
        FileName = None
        Attribute = None
        Type = None
        Address = None
        Size = None

[Variable]

Variable

Description

VariableName

This holds the variable name.

FileName

This holds the full path of the file that the variable is defined.

Attribute

This holds the attribute.

Type

This holds the type.

Address

This holds the address.

Size

This holds the size.

[Detailed description]

-

VariableInfo is a class, and it is the structure of the return value from the project.GetVariableList function.

[Example of use]

>>>info = project.GetVariableList()
var1 volatile int 0x000014e4 4 C:\project\src\test1.c
var2 static int 0x000014e8 4 C:\project\src\test2.c
>>>print info[0].VariableName
var1
>>>print info[1].FileName
C:\project\src\test2.c
>>>print info[0].Attribute
volatile
>>>print info[0].Type
int
>>>