Source


This function runs a script file.

[Specification format]

Source(scriptFile)

[Argument(s)]

Argument

Description

scriptFile

Specify the script file to run.

[Return value]

None

[Detailed description]

-

This function runs the script file specified by scriptFile.

-

This function operates the same as "execfile" of IronPython.

[Example of use]

>>>Source("../../testScriptFile2.py")
>>>Source("E:/TestFile/TestScript/testScriptFile.py")
>>>