This property refers to the nickname of the microcontroller of the active project.
[Specification format]
[Setting(s)]
None
[Reference]
Nickname of the microcontroller of the active project
[Detailed description]
- | This property refers to the nickname of the microcontroller of the active project. |
[Example of use]
>>>print project.Nickname
RL78/G13 (ROM:64KB)
|