B.3.10 CS+ Python property (for debug tool)

Below is a list of CS+ Python properties (for the debug tool).

Table B.10

CS+ Python Property (For Debug Tool)

Property Name

Function Description

debugger.ActionEvent.GetLine

This property sets or refers to the number of action event results.

debugger.ADConvertDataInExecution

This property sets or refers to data collected in debugging.

debugger.Download.Property

This property sets or refers to conditions of the download file of the debug tool.

debugger.Interrupt.ExceptionCause

This property refers to the exception cause code.

debugger.IsMulticore

This property checks whether or not the microcontroller of the active project is multi-core.

debugger.Memory.NoVerify

This property switches the write-time verification setting.

debugger.Option.AccessDuringExecution

debugger.Option.AccessStopExecution

debugger.Option.AccumulateTraceTime

debugger.Option.AfterTraceMemoryFull

debugger.Option.Coverage

debugger.Option.MainClockFrequency

debugger.Option.OpenBreak

debugger.Option.ReuseCoverageData

debugger.Option.Timer

debugger.Option.Trace

debugger.Option.TraceBranchPC

debugger.Option.TraceDataAccess

debugger.Option.TracePriority

debugger.Option.TraceTarget

debugger.Option.UseTraceData

This property sets or refers to the options of the debug tool.

debugger.ProcessorElement

This property sets or refers to the PE of the multi-core.

debugger.XTrace.Addup

debugger.XTrace.Complement

debugger.XTrace.Mode

This property sets or refers to the tracing options of the debug tool.