debugger.XTrace.Addup
debugger.XTrace.Complement
debugger.XTrace.Mode
|
This property sets or refers to the tracing options of the debug tool. [IECUBE][IECUBE2][Simulator]
[Specification format]
debugger.XTrace.Addup = addup [Simulator]
debugger.XTrace.Complement = complement [IECUBE[V850]][IECUBE2[V850]]
debugger.XTrace.Mode = traceMode [Simulator][IECUBE][IECUBE2]
|
[Setting(s)]
|
|
addup
|
Set whether to add up times/tags.
True: Add up times/tags.
False: Do not add up times/tags.
|
complement
|
Set whether to supplement the trace.
True: Supplement the trace.
False: Do not supplement the trace.
|
traceMode
|
Set the trace control mode.
The trace control modes that can be specified are shown below.
|
|
|
TraceMode.FullBreak
|
Stop program execution and writing of trace data after all trace data has been used up.
|
TraceMode.FullStop
|
Stop writing trace data after all trace data has been used up.
|
TraceMode.NonStop
|
Continue writing trace data even if all trace data has been used up.
|
[Reference]
Set value
Caution | If a PM+ workspace is converted to a CS+ project, then there will be no debugging tool in the main project. For this reason, "None" will be returned if the main project is the active project. |
[Detailed description]
- | This property sets or refers to the tracing options of the debug tool. |
[Example of use]
>>>print debugger.XTrace.Addup
False
>>>debugger.XTrace.Addup = True
>>>print debugger.XTrace.Addup
True
>>>
|