This property sets and displays the setting for enabling or disabling the function for linking to an external tool at CS+ startup.
Set whether to enable or disable the function for linking to an external tool at CS+ startup. True: Enable the function for linking to an external tool (default). False: Disable the function for linking to an external tool. This will be True if the common.EnableRemotingStartup property is set to True on startup, and False otherwise. |
This property sets and displays the setting for enabling or disabling the function for linking to an external tool at CS+ startup. |