Renesas Electronics
Below is a list of the panel related to the Python console.
Table A.1
Panel List
Panel Name
Function Description
Python Console panel
This panel is used to use IronPython to control CS+ and the debug tool via the command input method.