CS+ is a integrated development environment that provides an environment for developing microcontrollers from creation of pin lists to code generation, build and debug all in one tool.
Easy system development
Use the Pin configuration function to create device top views and pin lists by selecting multi-purpose pins and used/unused pins. Using the code generating function, a program for implementing peripheral functions built in the microcontroller can be automatically generated just by selecting the items or entering numerical values even when you don't know the name of register or method of configuration. |
Easy GUI customization
You can customize the screen as you like using such features as "docking", "floating" or "automatic hiding" to manipulate various panels of CS+ at will. CS+ now provides a function to save the development environment in addition to the conventional function to save the project environment. All of these features help you develop a microcontroller system more smoothly. |
Easy installation
Since the development environment for system development is integrated, it is easy to install the required tools. Because it is equipped with an automatic update function, you can update the software to its latest version (including documents) with a single click. |