Generating code

2. Port configuration

In this step, you configure the functions of the Port.

Double-click the [Port] from [Code Generator (Design Tool)] in the Project Tree. This opens the panel for the port.

Select the [Port6] tab and configure as shown below.

In this step, you decide which pins to use. Refer to the circuit diagram shown below. Bit 2 and bit 3 of the port 6 are used as outputs. In QB-R5F100LE-TB, these are connected to LED1 and LED2 respectively.